Hardware requirements#
Micro USB cable
RT700 board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J54) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows example output of the MRT driver demo in the terminal window:
Starting channel No.0 ...
Channel No.0 interrupt is occured !
Channel No.0 interrupt is occured !
Channel No.0 interrupt is occured !