Hardware requirements#
Micro USB cable
MIMXRT685-AUD-EVK board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the example in the terminal window:
OTFAD example started!
Hitted context: 0x0
Erasing Serial NOR over FlexSPI...
Erase sector finished !
Decrypted data - successfully.
Note:
To generate ciphertext, you can use OTFAD_GetEncryptedCounter() and OTFAD_EncryptData() API in example[selected] or other library.
1. use OTFAD_GetEncryptedCounter() API get encrypted counter.
2. use encrypted counter XOR plaintext to generate ciphertext.