Hardware requirements#
Micro USB cable
MIMXRT685-AUD-EVK board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the shell demo in the terminal window:
SHELL (build: Aug 21 2018)
* Copyright 2021 NXP
SHELL>> help
"help": Lists all the registered commands
"led arg1 arg2":
Usage:
arg1: 1|2|3|4... Led index
arg2: on|off Led status
"exit": Exit program
SHELL>> led 1 on
SHELL>> led 2 off
LED index is wrong
SHELL>>