Hardware requirements#
Type-C USB cable
MCX-W72-EVK Board
Personal Computer
Board settings#
This example project uses LPCMP0 to compare the voltage signal input from channel 0(PTA4) with the voltage signal(half of VREF_OUT) output by LPCMP’s internal DAC. The voltage signal input from PTA4 corresponding J4-5 should be used to observe the dynamical IO state. You will see the red led toggle with the voltage change.
Prepare the Demo#
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
LPCMP polling Example.