Hardware requirements#
Mini/micro USB cable
MCXW23-EVK Board
Personal Computer
Board settings#
Use the default jumper settings.
Prepare the Demo#
Connect a USB cable between the host PC and the EVK board J33.
Open a serial terminal with the following settings
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build and download the application
Start a debug session or press the reset button
Running the demo#
The clock can be measured with an oscilloscope on J21-2.
The log below shows the output of the clockout demo in the terminal window:
Clock Output Driver Example.
Please choose one output clock.
A -- Main Clock.
B -- CLKIN Clock.
C -- FRO 32 MHz Clock.
D -- FRO 1 MHz Clock.
E -- FRO 24 MHz clock.
F -- Oscillator 32 kHz Clock.