MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • MCXW23-EVK Board

  • Personal Computer

Board settings#

Use the default jumper settings.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the EVK board J33.

  2. Open a serial terminal with the following settings

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Build and download the application

  4. Start a debug session or press the reset button

Running the demo#

When the demo runs successfully, the terminal displays similar information like the following:


CDOG Peripheral Driver Example

CDOG IRQ Reached
* Miscompare fault occured *

intruction timer:   fffc5
intruction timer:   c615e
intruction timer:   8c34e
intruction timer:   5251a
intruction timer:   18703
......
CDOG IRQ Reached
* Timeout fault occured *

End of example

Note: To keep the program running correctly, it is recommended to perform a power on reset (POR) after loading the application. SW reset does not clear pending fault flags.