Hardware requirements#
Mini/micro USB cable
MCXW23-EVK Board
Personal Computer
Board settings#
Use the default jumper settings.
Prepare the Demo#
Connect a USB cable between the host PC and the EVK board J33.
Open a serial terminal with the following settings
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build and download the application
Start a debug session or press the reset button
Running the demo#
The log below shows the output of the Casper example in the terminal window:
ModExp Test pass.
Casper ECC Demo P256
Round: 0
Round: 1
Round: 2
Round: 3
Round: 4
Round: 5
Round: 6
Round: 7
All EC scalar multiplication tests were succesfull.
Round: 0
Round: 1
Round: 2
Round: 3
Round: 4
Round: 5
Round: 6
Round: 7
All EC double scalar multiplication tests were succesfull.
Casper ECC Demo P384
Round: 0
Round: 1
Round: 2
Round: 3
Round: 4
Round: 5
Round: 6
Round: 7
All EC scalar multiplication tests were succesfull.
Round: 0
Round: 1
Round: 2
Round: 3
Round: 4
Round: 5
Round: 6
Round: 7
All EC double scalar multiplication tests were succesfull.
Casper ECC Demo P521
Round: 0
Round: 1
Round: 2
Round: 3
Round: 4
Round: 5
Round: 6
Round: 7
All EC scalar multiplication tests were succesfull.
Round: 0
Round: 1
Round: 2
Round: 3
Round: 4
Round: 5
Round: 6
Round: 7
All EC double scalar multiplication tests were succesfull.