Hardware requirements#
Mini/micro USB cable
MCX-N9XX-EVK board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, will get the similar messages on the terminal.
TRDC example start
Set the MBC selected memory block not accessible
Resolve access error
The MBC selected block is accessible now
TRDC example Success