Hardware requirements#
Micro USB cable
MCX-N5XX-EVK board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the host PC and the MCU-Link USB port (J5) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows example output of the MRT driver demo in the terminal window:
Starting channel No.0 ...
Channel No.0 interrupt is occurred !
Channel No.0 interrupt is occurred !
Channel No.0 interrupt is occurred !