Hardware requirements#
USB Type-C cable
MCIMX93-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo#
When the example runs successfully, you can see the similar information from the terminal as below.
Lpuart polling example
Board will send back received characters