MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MC56F80000-EVK board

  • Personal Computer

Board hardware common setting#

  1. Power setting:

    Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2

  2. Reset pin setting:

    Connect J11 pin2 and pin3

  3. Debugger setting:

    Connect J13 pin 1-2, 3-4, 5-6, 7-8

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with Multilink debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs successfully, the log would be seen on the terminal like:

QSCI polling example
Board will send back received characters
Please input one character at a time