Hardware requirements#
Micro USB cable
LPCXpresso860MAX board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows example output of the WKT driver demo in the terminal window:
WKT interrupt example
Self-wake-up timer interrupt is occurred !
Self-wake-up timer interrupt is occurred !
Self-wake-up timer interrupt is occurred !
Users can see that LED is blinking.