MCUXpresso SDK Documentation

Hardware requirements#

  • LPCXpresso 55S69 board

  • Mini/micro USB cable

  • Personal Computer

Board settings#

No special HW settings are required.

In case of MCUBoot for LPC55S69 there is currently no image revert mechanism. This is due to Flash ECC capability that doesn’t allow incremental flash programming. MCUBoot’s revert strategies rely on this mechanism, therefore it’s not currently practical to use any of the MCUBoot’s revert strategies like image swapping by move or stratch area.

MCUBoot memory layout#

Region

From

To

Size

MCUboot code

0x00000000

0x0001FFFF

128kB

Primary slot

0x00020000

0x0004FFFF

192kB

Secondary slot

0x00050000

0x0007FFFF

192kB

  • MCUBoot header size is set to 1024 bytes

  • Signing algorithm is ECDSA-P256

  • Write alignment is 4 bytes

  • MCUBoot is configured to use its OVERWRITE_ONLY image handling strategy

Image signing example#

imgtool sign   --key sign-ecdsa-p256-priv.pem
               --align 4
               --version 1.1
               --slot-size 0x30000
               --header-size 0x400
               --pad-header
               ota_mcuboot_basic.bin
               ota_mcuboot_basic.SIGNED.bin