Hardware requirements#
Micro USB cable
LPCXpresso55s69 board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the host PC and the LPC-Link USB port (P6) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows example output of the RTC driver demo in the terminal window:
RTC example: set up time to wake up an alarm
Current datetime: 2014-12-25 19: 0: 0
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19: 0: 5