Hardware requirements#
Micro USB cable
LPCXpresso55S28 board
Personal Computer
Board settings#
Master_board(SPI7) Slave_board(SPI2)
Pin Name Board Location Pin Name Board Location
MISO P17 pin 12 MISO P18 pin 6
MOSI P17 pin 10 MOSI P18 pin 10
SCK P17 pin 14 SCK P18 pin 8
SSEL1 P17 pin 1 SSEL0 P17 pin 16
Prepare the Demo#
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
SPI one board interrupt example started!
SPI transfer finished!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~