Hardware requirements#
Mini/micro USB cable
LPCXpresso55S28 board
Personal Computer
Board settings#
Connect a DC voltage source to P19_6 (PIO0_0/CMP IN1)
Prepare the Demo#
Note: MCUXpresso IDE project default debug console is semihost
Connect a macro USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
CMP interrupt driver example.
Then change CMP analog input, and the LED GREEN will show the output of the comparator. - Let CMP IN1 voltage be higher than half of the VDDA, LED GREEN on. - Let CMP IN1 voltage be lower than half of the VDDA, LED GREEN off.