MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • LPCXpresso55S16 board

  • Personal Computer

Board settings#

The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

The log below shows the output of the clockout demo in the terminal window:

Clock Output Driver Example.
Please choose one output clock.
        A -- Main Clock.
        B -- PLL0 Clock.
        C -- CLKIN Clock.
        D -- FRO 96 MHz Clock.
        E -- FRO 1 MHz Clock.
        F -- PLL1 clock.
        G -- Oscillator 32 kHz clock.

To measure the output clock signal, please use the oscilloscope to probe J7_6(J9_14).