Hardware requirements#
Mini/micro USB cable
LPCXpresso55S06 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
After the board is flashed the Tera Term will print message on terminal.
Example output:
AES ECB Test pass
AES CBC Test pass
AES CTR Test pass
SHA-1 Test pass
SHA-256 Test pass