Hardware requirements#
Mini/micro USB cable
LPCXpresso55S06 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows example output of the CRC driver demo in the terminal window:
CRC Peripheral Driver Example
Test string: 123456789
CRC-16 CCITT FALSE: 0x29b1
CRC-16 ARC: 0xbb3d
CRC-32: 0xcbf43926