Hardware requirements#
Two micro USB cables
LPCLPCXpresso54628 board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a micro USB cable between the host PC and the +5V Power only USB port on the target board (J1).
Connect a micro USB cable between the host PC and the Debug Link USB port on the target board (J8).
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows example output of the random number generator demo in the terminal window:
RNG Peripheral Driver Example
Generate 128-bit random number:
0x868516634E5D992656DA94C7BFAD956A
Press any key to continue...