Hardware requirements#
Micro USB cable
LPCXpresso54628 board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows example output of the RIT driver demo in the terminal window and see LED1 blinks at 1s period.
RIT Example Start, You will see spcified LED blink at 1s period interval.