Hardware requirements#
Mini USB cable
LPCXpresso51U68 board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
SHELL build: Sep 27 2020
Copyright 2020 NXP
LOG SHELL>> installbackend debugconsole
LOG SHELL>> log error
22350: ERROR log_main.c:104:This is "error" log message
LOG SHELL>> log fatal
27900: FATAL log_main.c:100:This is "fatal" log message
LOG SHELL>> log warning
35430: WARN log_main.c:108:This is "warning" log message
LOG SHELL>> log info
38585: INFO log_main.c:112:This is "info" log message
LOG SHELL>> log debug
41330: DEBUG log_main.c:116:This is "debug" log message
LOG SHELL>> log trace
45090: TRACE log_main.c:120:This is "trace" log message
LOG SHELL>> log test
49835: ERROR log_main.c:124:The input arguement "test" is not valid
LOG SHELL>> uninstallbackend debugconsole
LOG SHELL>>
Note: The shell information “SHELL build: Sep 27 2020” may be different, which depends on the compile date.