Hardware requirements#
Type-C USB cable
KW47-LOC Board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The J1 Pin 1 (ADC0_A15) on LOC board is used to monitor the voltage. The VREFO 1.8v is used as the ADC reference.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
LPADC Interrupt Example
ADC Full Range: 4096
Please press any key to get user channel's ADC value.
ADC value: 2714