Hardware requirements#
Micro USB cable
IMX95LPD5-EVK board
JLink Plus
12V~20V power supply
Personal Computer
Board settings#
No special is needed.
Prepare the Demo#
Connect 12V~20V power supply and JLink Plus to the board, switch SW4 to power on the board
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, following information can be seen on the terminal:
==FlexCAN loopback functional example -- Start.==
Send message from MB8 to MB9
tx word0 = 0x11223344
tx word1 = 0x55667788
Receved message from MB9
rx word0 = 0x11223344
rx word1 = 0x55667788
==FlexCAN loopback functional example -- Finish.==