MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • IMX95LPD5-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings#

No special settings are required.

Prepare the Demo#

  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo#

When the example runs successfully, you can see the similar information from the terminal as below.

==FlexCAN loopback functional example -- Start.==

Send message from MB0 to MB1
tx word0 = 0x0
tx word1 = 0x1
tx word2 = 0x2
tx word3 = 0x3
tx word4 = 0x4
tx word5 = 0x5
tx word6 = 0x6
tx word7 = 0x7
tx word8 = 0x8
tx word9 = 0x9
tx word10 = 0xa
tx word11 = 0xb
tx word12 = 0xc
tx word13 = 0xd
tx word14 = 0xe
tx word15 = 0xf

Received message from MB1
rx word0 = 0x0
rx word1 = 0x1
rx word2 = 0x2
rx word3 = 0x3
rx word4 = 0x4
rx word5 = 0x5
rx word6 = 0x6
rx word7 = 0x7
rx word8 = 0x8
rx word9 = 0x9
rx word10 = 0xa
rx word11 = 0xb
rx word12 = 0xc
rx word13 = 0xd
rx word14 = 0xe
rx word15 = 0xf

==FlexCAN loopback functional example -- Finish.==