Hardware requirements#
USB Type-C cable
i.MX943-EVK board
Personal Computer
Power supply 24V
Motor control board (FRDM-LVPMSM-FA)
EnDat3 sensor
Board settings#
Insert FRDM-LVPMSM-FA board into Arduino interface of motor control 2. Connect EnDat3 sensor and power supply to FRDM-LVPMSM-FA
EnDat3 connection:
INSTANCE(FRDM-LVPMSM-FA) CONNECTS TO INSTANCE(EnDat2.2 sensor)
Pin Name Board Location Signal Name
ENC_DATA_IO_P J70-4 DATA_P
ENC_DATA_IO_N J70-9 DATA_N
VENC J70-1 UP - Power supply voltage
GND J70-6 GND
SW90 setting:
SW[1-2] OFF:ON Half duplex
SW[3] OFF Echo Enabled
SW[4] ON ENDAT is used.
SW30 setting - Select the appropriate voltage based on the properties of the sensor
SW[1] ON 3.3V
SW[2] ON 5.2V
SW[3] ON 9V
SW[4] ON 12V
Jumpers:
J300: pin1 <--> pin2
Prepare the Demo#
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW1(SYS_PWR) to power on the board.
Connect a micro USB cable between the host PC and the J15(FTDI_DEBUG) USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.