MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • IMX943-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings#

No special settings are required.

Note#

Cannot get temperature from sensor temp_a55. It’s an expected behaviour.

Prepare the Demo#

  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo#

The log below shows the output of the hello world demo in the terminal window:

Temperature measurement example.
 desc[0].sensorId = 0x0
 desc[0].name = temp_ana
 desc[1].sensorId = 0x1
 desc[1].name = temp_a55
 desc[2].sensorId = 0x2
 desc[2].name = temp_pf09
 Pls input a number to choose sensor to get data:(valid input is 0-2)0
 Sensor(desc index is 0) temp_ana is selected
 Sensor is ready to read, press enter key to get the temperature.
 Current temperature is 39 degrees Celsius
 Pls input a number to choose sensor to get data:(valid input is 0-2)1
 Sensor(desc index is 1) temp_a55 is selected
 Sensor configuration failed!
 Pls input a number to choose sensor to get data:(valid input is 0-2)2
 Sensor(desc index is 2) temp_pf09 is selected
 Sensor is ready to read, press enter key to get the temperature.
 Current temperature is 105 degrees Celsius
 Pls input a number to choose sensor to get data:(valid input is 0-2)