MCUXpresso SDK Documentation

Hardware requirements#

  • Mini/micro USB cable

  • Personal Computer

Board settings#

Make sure the board is setup to boot from flash.

Default MCUBoot memory layout#

In all cases, the MCUBOOT bootloader reserves 256kB at the beginning of the external flash followed by 2MB slots for application. The resulting layout for the monolithic application will be as follows:

Region

From

To

Size

MCUboot code

0x08000000

0x0803FFFF

256kB

Primary slot

0x08040000

0x0821FFFF

2048kB

Secondary slot

0x08240000

0x0841FFFF

2048kB

  • MCUBoot header size is set to 1024 bytes

  • Signing algorithm is ECDSA-P256

  • Write alignment is 4 bytes

  • MCUBoot is configured to use its DIRECT_XIP image handling strategy together with FlexSPI flash remapping

  • For testing purposes, the image authentication may be disabled in sblconfig.h by uncommenting the CONFIG_BOOT_OTA_TEST definition so that the following is defined:

    #define MCUBOOT_NO_SIGN #define CONFIG_BOOT_HASH_NO_SIGN #define CONFIG_BOOT_DIGEST_TYPE_SHA256

Image signing example#

imgtool sign   --key sign-ecdsa-p256-priv.pem
               --align 4
               --version 1.1
               --slot-size 0x200000
               --header-size 0x400
               --pad-header
               ota_mcuboot_basic.bin
               ota_mcuboot_basic.SIGNED.bin

Note that for the first image flashed manually together with the bootloader additional imgtool options --pad and --confirm must be used. Otherwise the bootloader would reject the image for missing data in the trailer area.

Custom configuration - Encrypted XIP#

Region

From

To

Size

MCUboot code

0x08000000

0x0803FFFF

256kB

Primary slot

0x08040000

0x0821FFFF

2048kB

Secondary slot

0x08240000

0x0841FFFF

2048kB

Encryption metadata

0x08440000

0x08440FFF

4kB

This custom build generates a project with predefined configuration to utilize Encrypted XIP mode. For more information please see Encrypted XIP and MCUboot.

  • MCUBoot header size is set to 1024 bytes

  • Signing algorithm is ECDSA-P256

  • Write alignment is 4 bytes

  • MCUBoot is configured for Encrypted XIP mode using modified MCUBOOT_OVERWRITE_ONLY image update strategy

  • MCUboot uses ECDH-P256 to secure AES key for image encryption

  • Primary slot is encrypted by IPED module to utilize encrypted XIP

Image signing example:

imgtool sign --key sign-ecdsa-p256-priv.pem
             --align 4
             --version 1.1
             --slot-size 0x200000
             --header-size 0x400
             --max-sectors 59
             --pad-header
             -E enc-ec256-pub.pem
             ota_mcuboot_basic.bin
             ota_mcuboot_basic.SIGNED.bin

Project building example:

The project is built using west tool. For more information please see MCUXpresso SDK documentation.

Bootloader:

west build -p always examples/ota_examples/mcuboot_opensource --toolchain iar -t guiproject --config flash_debug -b frdmrw612 -DCONF_FILE="examples/ota_examples/_custom_cfg/rw61x/mcuboot_opensource.conf" -d builds/rw612_mcuboot

OTA application:

west build -p always examples/ota_examples/ota_mcuboot_basic --toolchain iar -t guiproject --config flash_debug -b frdmrw612 -DCONF_FILE="examples/ota_examples/_custom_cfg/rw61x/ota_mcuboot_basic.conf" -d builds/rw612_ota_mcuboot_basic