Hardware requirements#
Type-C USB cable
Personal Computer
FRDM-MCXW72 Board
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.