MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXW72 Board

  • Personal Computer

Board settings#

This Example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.

Prepare the Demo#

  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo#

These instructions are displayed/shown on the terminal window:

PFlash Example Start

PFlash Information:
Program Flash block bass address:	0, Hex: (0x0)
Program Flash block Size:		2048 KB, Hex: (0x200000)
Program Flash block Sector Size:	8 KB, Hex: (0x2000)
Program Flash block count Size:	1
Total Program Flash Size:		2048 KB, Hex: (0x200000)

Erase a sector of flash
Successfully Erased Sector 0x1fe000 -> 0x200000

Program a buffer to a phrase of flash 
Successfully Programmed and Verified Location 0x1fe000 -> 0x1fe010 

End of PFlash Example

And you will find the flash hase been programed.