Hardware requirements#
Type-C USB cable
FRDM-MCXW72 Board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
Status=DD000001, Reply=AA000002
OneCmd Blocking F32 MAT MULT Test Passed: Status=DD000002, Reply=AA000003
OneCmd Blocking CF32 MAT MULT Test Passed: Status=DD000003, Reply=AA000004
Blocking Cmd Queue Test Passed: Status= 0, Reply=AA000005