Hardware requirements#
Type-C USB cable
FRDM-MCXW23 Board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
Event task is running.
Receive message counter: 1.
Receive message counter: 2.
Receive message counter: 3.
Receive message counter: 4.
Receive message counter: 5.
Receive message counter: 6.
Receive message counter: 7.
Receive message counter: 8.
Receive message counter: 9.
Receive message counter: 10.
Receive message counter: 11.
Receive message counter: 12.
Receive message counter: 13.
Receive message counter: 14.
...