MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXW23 Board

  • Personal Computer

Board settings#

Prepare the Demo#

  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

The log below shows the output of the demo in the terminal window:

CRC Peripheral Driver Example

Test string: 123456789
CRC-16 CCITT FALSE: 0x29b1
CRC-16 ARC: 0xbb3d
CRC-32: 0xcbf43926