Hardware requirements#
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J17) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, the log would be seen on the terminal like:
Utick example start...
UTICK delay 1 second...
UTICK delay 1 second...