Hardware requirements#
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the hello world demo in the terminal window:
Press any key to start example.
Board will enter power deep sleep mode, and then wakeup by OS timer after about 5 seconds.
After Board wakeup, the OS timer will trigger the match interrupt about every 2 seconds.
Board wakeup from deep sleep mode.
OS timer match value reached
OS timer match value reached
OS timer match value reached