Hardware requirements#
Type-C USB cable
FRDM-MCXN947 Board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect the type-c and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
INTM Example Start:
Press SW3 to trigger interrupt.
INTM timeout.
INTM Example End.