Hardware requirements#
Type-C USB cable
FRDM-MCXL255 board
Personal Computer
Board settings#
Make sure you have solder bridges SJ1 and SJ2 set to
2-1 for the main core (cm33)
Prepare the Demo#
Connect a USB Type-C cable between the host PC and the MCU-Link USB port (J16) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The following lines are printed to the serial terminal when the demo program is executed.
==================================================
RTC Free Running Mode Example
==================================================
RTC initialized in Free Running Mode with initial counter value: 0.
Tamper 0 is enabled, press the button to trigger it.
Alarm 0 clock will ring every 2 seconds.
Alarm 1 clock will ring in the 5th second.
*** ALARM 0 occured! ***
*** ALARM 0 occured! ***
*** ALARM 1 occured! ***
*** ALARM 0 occured! ***
*** ALARM 0 occured! ***
*** ALARM 0 occured! ***
*** ALARM 0 occured! ***