Hardware requirements#
Type-C USB cable
FRDM-MCXE31B board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the terminal window:
--- Destructive reset test start ---
Destructive reset occurred!
--- CMU FC test start ---
Monitored clock works fine!