Hardware requirements#
Mini/micro USB cable
FRDM-MCXE31B board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, the following message will display in the terminal:
Copyright 2022 NXP
SHELL>> help
"help": Lists all the registered commands
"exit": Exit program
"led arg1 arg2":
Usage:
arg1: 1|2|3|4... Led index
arg2: on|off Led status
SHELL>> led 1 on
SHELL>> led 1 off
SHELL>> led 4 on
LED index is wrong
SHELL>>
Note: If the command ‘led x on’/’led x off’ run success, the corresponding LEDx on board will turn on/turn off. But the valid “Led index” may be different, which depends how many LEDs are available on the specific board. For example: one board only have LED1/LED2, then shell demo will print “LED index is wrong” for all led index bigger than 2.