Hardware requirements#
Type-C USB cable
FRDM-MCXC444 board
Personal Computer
USB to Com Converter
Board settings#
Connect pin:
RX of USB2COM to J1_6
TX of USB2COM to J2-4
GND of USB2COM to J2-14
Prepare the Demo#
Connect USB to Com Converter between the PC host and the port on the board.
Open a serial terminal on PC for serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the UART Terminal port which connected to the USB2COM like:
Uart functional interrupt example
Board receives characters then sends them out
Now please input: