Hardware requirements#
Type-C USB cable
FRDM-MCXC444 board
Personal Computer
Board settings#
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo#
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
These instructions are displayed/shown on the terminal window:
FLASH example Start
Flash Information:
Total Program Flash Size: xx KB, Hex: (xx)
Program Flash Sector Size: xx KB, hex: (xx)
...
Flash is xx
Erase a sector of flash
Successfully Erased Sector xx -> xx
Program a buffer to a sector of flash
Successfully Programmed and Verified Location xx -> xx
End of FLASH example