MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXC444 board

  • Personal Computer

Board settings#

No special is needed.

Prepare the Demo#

  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.

  2. Connect the analog signal source’s output to the input of used-defined comparator’s channel (defined as “DEMO_CMP_USER_CHANNEL” in source code.)

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Reset the SoC and run the project.

Running the demo#

When the demo runs successfully, the log would be seen on the terminal like:

CMP interrupt Example

Then change CMP analog input, and watch the change of LED. - CMP0_IN0 (Jump J1-9) connected to VCC=3.3V (Jump J3-8): LED RED on - CMP0_IN0 (Jump J1-9) connected to GND (Jump J2-14): LED RED off