Hardware requirements#
USB-C cable
FRDM-MCXC242 board
Personal Computer
Board settings#
No special board settings.
Prepare the Demo#
Connect a mini/micro USB cable between the PC host and the OpenSDA USB port on FRDM-MCXC242 board.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. For detailed instructions, see Getting Started with Software Development Kit for MCXC242.
Running the demo#
When the demo runs successfully, the board’s LED will blink.