Hardware requirements#
USB-C cable
FRDM-MCXC242 board
Personal Computer
Board settings#
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo#
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
These instructions are displayed/shown on the terminal window:
FLASH example Start
Flash Information:
Total Program Flash Size: xx KB, Hex: (xx)
Program Flash Sector Size: xx KB, hex: (xx)
...
Flash is xx
Erase a sector of flash
Successfully Erased Sector xx -> xx
Program a buffer to a sector of flash
Successfully Programmed and Verified Location xx -> xx
End of FLASH example