MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXC041 board

  • Personal Computer

Board settings#

No special board settings.

Prepare the Demo#

  1. Connect a Type-C USB cable between the PC host and the OpenSDA USB port on FRDM-MCXC041 board.

  2. Download the program to the target board.

  3. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. For detailed instructions, see Getting Started with Software Development Kit for MCXC041.

Running the demo#

When the demo runs successfully, the board’s LED will blink.