MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • FRDM-MCXA366 board

  • Personal Computer

Board settings#

Prepare the Demo#

  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo#

The log below shows the output of the trng example in the terminal window:

TRNG Peripheral Driver Example
Generate 10 random numbers: 
Random[0] = 0x201FEB53
Random[1] = 0x85A32C28
Random[2] = 0xDC66342C
Random[3] = 0xFD43ACFF
Random[4] = 0x1CD53C0
Random[5] = 0xB27EDBEB
Random[6] = 0x32AB81D5
Random[7] = 0x6AA5B70F
Random[8] = 0x81C41286
Random[9] = 0xC9620BD8

 Press any key to continue...