Hardware requirements#
Type-C USB cable
FRDM-MCXA344 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a USB cable between the host PC and the EVK board J21.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, will get the similar messages on the terminal.
TRDC example start
Set the MBC selected memory block not accessiable
Resolve access error
The MBC selected block is accessiable now
TRDC example Success