Hardware requirements#
FRDM-MCXA153 board
USB-C cable
Personal Computer
Board settings#
MCUBoot layout#
Region |
From |
To |
Size |
|---|---|---|---|
MCUboot code |
0x00000000 |
0x00006000 |
24kB |
Primary slot |
0x00006000 |
0x00011FFF |
48kB |
Secondary slot |
0x00012000 |
0x0001DFFF |
48kB |
Optional data |
0x0001E000 |
0x0001FFFF |
8kB |
MCUBoot header size is set to 512 bytes
Signing algorithm is ECDSA-P256
Write alignment is 16 bytes
Used
OVERWRITE_ONLYimage strategy due to limited flash sizeA large sector size of 8kB needs to be considered when allocating space for the image trailer as this needs to be sector aligned. This reduces the usable space for the application to only 40kB.
Image signing example#
imgtool sign --key sign-ecdsa-p256-priv.pem
--align 16
--version 1.1
--slot-size 0xc000
--header-size 0x200
--pad-header
ota_mcuboot_basic.bin
ota_mcuboot_basic.SIGNED.bin
If you experience problems with flash erase, check correct configuration
of ACL_SEC_x fields in CMPA region.