MCUXpresso SDK Documentation

Hardware requirements

Hardware requirements#

  • Micro USB cable

  • FRDM-KE17Z board

  • Personal Computer

Board settings#

This example project uses ADC12 instance 0 to sample and convert the voltage signal input from channel 0(PTE9). So the voltage signal input from PTE9(J3-3) should be changed to observe the dynamical conversion result.

Prepare the Demo#

  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.