Hardware requirements#
Micro USB cable
FRDM-KE16Z board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
SCG Example Start
SCG clock source frequency
SIRC clock: 8000000 Hz
FIRC clock: 48000000 Hz
LPFLL clock: 48000000 Hz
Current power mode: VLPR
Core clock: 4000000 Hz
Slow clock: 1000000 Hz
Current system clock: RUN
Core clock: 48000000 Hz
Slow clock: 24000000 Hz
Current power mode: RUN
Core clock: 8000000 Hz
Slow clock: 4000000 Hz
SCG Example End.